___________________________________________________________________________
README      Example 64-bit Fixed-Point Single Channel SISD IIR

Analog Devices, Inc.
DSP Division
P.O. Box 9106
Norwood, MA 02062

25-June-2005

This directory contains the source files for a single channel SISD IIR
filter for the SHARC DSP. All of the data files are in 64-bit hex format.

Files contained in this directory:

21367_IVT.asm           Interrupt Vector Table for the ADSP-21367
ADSP-21367-EZKIT.ldf    Linker Description File set up for the ADSP-21367
asm64 IIR.dpj           VisualDSP++ 4.0 Project File for this example
coeffs.dat              Filter Coefficients
expected_output.dat     Expected output when using provided input
iir64.asm               Filter Source Code
inwave.hex              Input Data
readme.txt              This file